Cart  |  Contact  |  Help  |  auinfo@dwyeromega.com  | 
Toll-Free in Australia: 1800 106 210
International+65 6415 5353

Wireless Sensors

Introduction to Wireless Sensors

Wireless sensors are standard measurement tools equipped with transmitters to convert signals from process control instruments into a radio transmission. The radio signal is interpreted by a receiver which then converts the wireless signal to a specific, desired output, such as an analog current or data analysis via computer software.

OMEGA Engineering offers a wide range of wireless sensors in Australia.

What are the primary benefits to using wireless sensors?

Safety
Wireless instruments can be used in locations that are difficult to access due to extreme conditions such as high temperature, pH, pressure, etc. Using wireless sensors, operators can continuously supervise processes in hazardous environments and report the data back to an operator in a monitoring facility located at a safe distance away. Wireless measurement is also useful for obtaining data in hard to access locations.

Convenience
Wireless sensors can be used to form a web/network that would allow an engineer to monitor a number of different locations from one station. This provides a centralized control of a factory. Additionally, a number of wireless sensors have the ability to create a unique web page making up-to-the-minute data, accessible anywhere in the world.

Reduce Costs
Wireless process control can reduce the cost of monitoring and running a factory by eliminating the need for extension wire, conduit, and other costly accessories.

All of OMEGA's wireless products expand upon the capabilities of traditional wired sensors and controllers. OMEGA's extensive line of products includes wireless meters and transmitters that have built-in displays, alarms, and controllable outputs. Switching to wireless instruments will provide convenience and capability.

Selecting a Wireless Sensor

There are a number of items to consider when selecting a wireless measurement instrument.

Type of Measurement: It is important to understand what is being measured. Wireless transmitters (which incorporate wireless process measurement and control) typically have a unique function. Sensors are specifically designed for temperature, pressure, flow, etc., and must be selected accordingly.

Accuracy and Response Time: How accurate does the measurement need to be, and how quickly should the measurement be updated? Most wireless sensors are as accurate as their wired counterparts; however the readings are typically transmitted every few seconds to preserve battery power. If instantaneous measurement is necessary, this must be taken into consideration when selecting the wireless transmitter because certain models may not offer the desired response time.

Range: The range of wireless sensors varies widely. Some are designed for short-range, indoor applications of a few hundred feet, while other sensors can transmit data to a receiver located miles away. Regardless of the sensors capability, the range of a wireless signal is always limited by obstructions. Transmitting through machines, walls, and structures degrades signal strength and reduces range capability. As a result, the range of a transmitter located indoors is typically significantly less than the same transmitter broadcasting outside in wide open field.

Frequency: The frequency of radio transmission is also important to consider. Laws vary by country and region as to which parts of the wireless spectrum are available for use without specific licenses. In the USA 915MHz, 2.4GHz (WiFi) are the major frequencies factories can use to transmit signals. As part of the industrial, scientific, and medical band, users do not need a radio license to operate on these frequencies. In Europe, wireless products typically operate on 868MHz or 2.4GHz. Due to regulatory requirements, products may only be available in certain regions.


Choose the right wireless sensor for your application

Top
Wireless Transmitters Wireless Transmitters
Transmitters use scientific sensors such as thermocouples, pressure transducers, flow meters, etc. to measure a specific property in a process, and then transmit the data via radio signals to a receiver.
Wireless Receivers Wireless Receivers
Receivers receive and interpret the wireless data. The receiver 'reads' a radio signal and converts it into the desired output such as contact closure, analog output, or digital display; some receivers can even export the data to advanced software.
Wireless Controllers Wireless Controllers
Controllers function similar to a receiver in the sense that they receive and analyze data from wireless transmitters. However, the wireless controllers are also able to manipulate a process based on the data being measured. For example, if a furnace becomes too hot, a controller can recognize the increased temperature and send a signal to turn off some heating elements.
Wireless Data Loggers Wireless Data Loggers
Data Loggers form a special type of wireless measurement network because they give a new dimension of flexibility to the end user. Wireless data loggers can remotely monitor temperature anywhere and then transmit the data back to an engineer once the unit is brought to a receiver. These miniature wireless sensors are useful for applications that involve a roaming element, such as food being shipped. By packaging a wireless data logger within a shipping container, a vendor or transporter can ensure and certify that products were refrigerated all the way to a distributor or grocery store.
Wireless Data Loggers Transceivers
Transceivers contain a transmitter and receiver in a single unit. The ability to rebroadcast signals makes wireless transceivers able to extend the range of your wireless measurement network.

Shop for Wireless Sensors in Australia

The OMEGA Engineering Singapore office handles all inquiries and orders for Australia. We have Application Engineers and Sale Support Staff ready to assist you with your technical questions, quotations and orders. A one-stop source for process measurement and control, OMEGA provides support through web chat, e-mail and telephone. View our contact page to call or email us.